오늘 무엇을 도와드릴까요?

[M580 Hardware] Is there any maintenance task is required for the M580 CPU?

M580 CPU has no battery, no fan,but it'd better to blow away the dust on the shell surface and check the LED status of CPU regularly.