오늘 무엇을 도와드릴까요?

How do you add the Fast Device Replacement or FDR name on the ATV32 drive with the optional ethernet card installed?

Issue:
Adding Fast Device Replacement or FDR name on the ATV32 with the optional ethernet card

Product Line:
Altivar ATV32

Environment:
All

Cause:
Wants to add a FDR name to the Drive

Resolution:
You can access the FDR device name two ways. The free Somove software or directly on the drive if you have the optional VW3A1101 HMI.

1.) Somove software using the Ethernet cable or optional TCSMCNAM3M002P cable under the parameters tab you will see FDR.
Click on the faulty device replacement
Activate the FDR by checking the box
Add your FDR IP address
Add your Device name at the bottom.
or
2.) If you have the remote graphic HMI VW3A1101 + the remote bezel VW3A1102 or the optional RJ45 adaptor with cable (VW3A1104R10)