브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
		
오늘 무엇을 도와드릴까요?
Video: How to change the Coil Fluid Temperature Thresholds on a Network Air FM Unit
Issue:
This document contains a video of how to change the Coil Fluid Temperature Thresholds on a Network Air FM Unit.

Product line:
FM 35-50, IR40, ACFM400, ACFM200.

Environment:
All Serial Numbers.

Cause:
Install, Configuration.

Resolution:



To change or set the coil fluid temperature threshold.

Press the ESC Key until you get to the main menu.

Press ENTER on Setup.

Press ENTER on System 1.

Press ENTER on Alarms.

Scroll down to Coil Fluid Thrshlds and press ENTER.

Using the UP or DOWN arrows you can select the High or Low threshold.

Press ENTER on either then change the value with the UP or DOWN arrow.

Finish by pressing the ENTER key and then press ESC until you get to the status menu.