오늘 무엇을 도와드릴까요?

What is the difference between an ATV930 part number and an ATV930 part number with "C" at the end?

Issue:
Meaning of the C suffix on an ATV930.

Product Line:
ATV930 series

Environment:
All models, All serial numbers

Cause:
Feature clarification

Resolution:
The ATV930 series drives without the "C" on the end include an internal braking transistor.
If the part number has a "C" at the end, the braking transistor is not included.  To use a braking resistor, a separate braking unit must be purchased separately.