오늘 무엇을 도와드릴까요?

Modbus TCP IO scanner for SoMachine

Issue:
Does SoMachine V3.1 or V4.1 offer a Modbus TCP IO scanner for SoMachine controllers?

Product Line:
M258, M241, M251

Resolution:
Modbus TCP and Ethernet/IP IO scanner are only possible on the M251 controller since SoMachine V4.1 and on some M241 controllers since SoMachine V4.2.
The M258 and LMC058 controllers only offer serial Modbus IO scanner.