When using 3 or 4 wire RTD's the maximum distance between the module and the sensor is 200 meters.
If you're using 2 wire RTD's the distance is limited only by the user defined accuracy of the application.
If you're using 2 wire RTD's the distance is limited only by the user defined accuracy of the application.
게시 대상: 슈나이더 일렉트릭 Korea