오늘 무엇을 도와드릴까요?

Why the island node configuration of STB is blank when it is opened from Unity Pro NOE I/O scanning STB DTM tab through zef ?

The zef file doesn't include the STB configuration information inside of NOE I/O scanning field ,so the blank page will be opened if you active the STB DTM through I/O scanning.
There are two solutions could be used
1> Customer could save the old application as sta format and reopen it in newer Unity Pro ,all the STB information are included
2>copy the previous STB configuration files (*.isl ) to current unity import/export folder ,open the zef file and all STB info could be visible.