오늘 무엇을 도와드릴까요?

SoMachine vs SoMachine Basic

Issue:
Difference between SoMachine and SoMachine Basic

Product Line:
SoMachine, SoMachine Basic

Resolution:
SoMachine Basic is a free software created specifically to program the M221 Logic Controller exclusively.
It supports the Ladder and the Instruction List programming languages.

SoMachine is a full blown licensed software used to program a wide range of controllers like the M241, M251, M238, M258, LMC058, LMC078... as well as the Maglis HMIs.
It supports all of the IEC61131-3 programming languages.