How to configure PME to work with HTTPS with SSL enabled?
Issue
Enabling SSL on the PME webpage and requiring HTTPS causes the webpage to no longer work.
Product Line
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024
Environment
Web Applications
Cause
The PME webpage uses hard coded HTTP links in the various web.config files. When the webpage is set to require HTTPS within IIS, the website breaks due to these links.
Resolution
The attached documents details the steps required to enable HTTPS with SSL encryption.
Recommendation
If you are using an older version of PME, consider upgrading to the latest version for improved protocol support and security. For assistance with integration or upgrades, contact Schneider Electric Technical Support at: pmo.support@se.com