How do you protect the drive from users accessing menus on the ATV61 and ATV71 drive?
Issue:
Protect access of the ATV61/ATV71 menus.
Product Line:
Altivar 61, Altivar 71
Environment:
All
Cause:
Protection.
Resolution:
This function is available under 7.3.
You can either choose to protect or make invisible entire menus or select the parameters needed.
Protect access of the ATV61/ATV71 menus.
Product Line:
Altivar 61, Altivar 71
Environment:
All
Cause:
Protection.
Resolution:
This function is available under 7.3.
You can either choose to protect or make invisible entire menus or select the parameters needed.