오늘 무엇을 도와드릴까요?

Which version of wonderware client/drive will be compatible with OFS V3.6

Question:
Which version of wonderware client/drive will be compatible with OFS V3.6?

Answer:
Regarding compatibility, there is not known  issue of OFS regarding OPC DA 2.04 compatibility
If Wonderware Client/Drive is also compatible with  OPC DA 2.04, the compatibility with OFS should be ok