What are the key features of PM3200 series meters ?
Issue
What are the key features of PM3200 series meters?
Product Line
PowerLogic PM3200 Series
Environment
PM3200 Series Energy Meters – Features Overview
Resolution
The key features of the PM3200 series meters include:
- Monitoring of electrical parameters such as I, In, U, V, P, Q, S, E, PF, Hz
- Power/current demand and peak demand measurement
- Time-stamped alarms for event tracking
- Minimum/maximum values for multiple parameters
- Management of up to 4 tariffs
- Up to 2 digital inputs and 2 digital outputs
- Modbus communication for integration with monitoring systems