How can I use the Dual Phase Counting Mode on BMXEHC0800(H) in X80 EIO drop ?
In order to support the Dual Phase Counting Mode on BMXEHC0800(H) in X80 EIO drop ,customer needs to upgrade this module at least to SV1.20 .
The module type should be selected to BMXEHC0800.2 in Unity Pro to include this feature.
The module type should be selected to BMXEHC0800.2 in Unity Pro to include this feature.