I need to replace LMC Pro, Pro2 controller. How to transfer the program?
There are several options:
1) Firmware and the software is stored on CF card. When you need to replace a PacDrive controller, you can keep the old CF card (program is saved here) and use it in new on.
2) If you have a backup created, you can download it to the new controller with Controller assistant software.
3) If you have source files of the application you can download it to the controller wit SoMachine Motion or Machine Expert.