오늘 무엇을 도와드릴까요?

Does the ATS22 have a timed logic input available?

Issue:
Time delay on an ATS22 start input.

Product Line:
Altistart 22, ATS22

Environment:
all

Cause:
n/a

Resolution:
The ATS22 does not offer a time delay feature to the logic inputs.  If a delay is required, use an external timer.