브랜드

Impact-Company-Logo-English Black-01-177x54

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
		
오늘 무엇을 도와드릴까요?
Is Energy Monitoring affected when applying single phase line voltage to an ATV630?
Issue:
Using single phase input voltage will affect energy monitoring?

Product Line:
Altivar 630 drives

Environment:
All

Cause:
Need details of energy monitoring in single phase environment

Resolution:
Yes, using single phase input voltage will affect energy monitoring.

The energy monitoring functionality is based on nominal current drive with error estimation +/- 5% .
Please review the Annex document for ATV630 drives (https://www.se.com/us/en/download/document/EAV64300/ ) for specific details when attempting to use an ATV630 drive with single phase input.
Because a drive being used with single phase input voltage must be oversized to be able to provide sufficient power to a 3 phase motor, the margin for error will be much bigger, and so the energy monitoring is far from reality.
If measuring is needed, an external device would have to be used (like a PowerLogic for example).