오늘 무엇을 도와드릴까요?

Is the BMENOC0301 module hot swappable?

Issue
Desire to replace the NOC without impacting the CPU.

Product line
Modicon M580

Resolution
The BMENOC0301 module can be replaced simply by removing the cables, lifting it out of the backplane then dropping the new one in and replacing the cables. It will receive the configuration from the M580 after booting up.

Your network will now include an Ip address that has changed its MAC address. This may or may not raise a flag depending on your specific installation.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)