How can I activate / deactivate a driver in Vijeo Designer associated to a PLC?
You can write the values 1 or 0 to turn on (1) or off (0) the communication with the associated equipment. A value of 2 indicates the driver is offline for this specific equipment.
When State is 0, communication with the associated equipment has stopped.
When State is 1, there is ongoing communications with the associated equipment.
When State is 2, the driver is offline for this specific equipment. The driver has attempted to communicate with the associated equipment but has timed out for the final time.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: