오늘 무엇을 도와드릴까요?

What would cause the ATV630 outdoor drive not to start the motor in auto mode?

Issue:
ATV630 HOA is not starting in auto mode.

Product Line:
ATV630 Outdoor Drive only

Environment:
All

Cause:
Customer supplied auto start contact is open

Resolution:
Close field terminal block 208 and 208