오늘 무엇을 도와드릴까요?

What can cause a LCF (Line contactor failure) on the Altivar Process Drive ATV630 and ATV930?

Issue:
What is the fault code LCF on the ATV630 and ATV930 drives?

Product Line:
ATV630  ATV930

Environment:
All serial numbers

Cause:
Customer said the drive had a fault code LCF.

Resolution:
The fault takes place as soon as the line contactor is not closed after a defined time (LCT).
This function allows the line contactor to close and open depending on the start/stop command.
Check the line contactor and its' wiring.
Check parameter LCT (Mains Voltage.time out) under Complete setting -> Generic functions -> Mains contactor comm -> Mains V. time out.
If there is a timing issue, try to increase this value.
The Mains Voltage time out is factory set to 5s.