오늘 무엇을 도와드릴까요?

How to analyze the issue of operation successful bit of PID block freeze?

  1. Issue
The operation successful bit of PIDFF block will go to 0 and freeze when switch the mode of PIDFF block from Manual Mode to Auto Mode.
  1. Product Line
M580
  1. Environment
Control Expert V14.0, Windows 10 64Bit
  1. Resolution
Slow down the frequency of the enable bit of PIDFF block, then the issue will not occur.