오늘 무엇을 도와드릴까요?

Does HMISCU support 187500bps if using MPI/PPI Driver in VJD

  1. Issue
Does HMISCU support 187500bps if using MPI/PPI Driver in Vijeo Designer 6.2?
  1. Environment
Vijeo Designer 6.2.
  1. Resolution
No,HMISCU target machines support 9600 and 19200 bps only if it is MPI/PPI Driver.