오늘 무엇을 도와드릴까요?

Why does Control Expert v14.0 generate a linking error when linking a PROCESS section variable to a SAFE section variable?

This error occurs when the customer:

  • uses Control Expert 14.0
  • loads an already-built application
  • adds new variables in a Process section and in a SAFE section
  • links the variables
  • run a "build change"


Possible workarounds :

  • export to .zef format, and reimport
  • run a build-all instead of a build-change


This bug was fixed in Control Expert 14.1