브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
		
오늘 무엇을 도와드릴까요?
What can cause an InFN or error 23 fault on the ATV630 or ATV930 Process drives?
Issue:
InFN or error 23 fault on the Process drives.

Product Line:
ATV 630, 930 680 980 etc

Environment:
All

Cause:
A communication interruption between the control block and the AFE or the BU bricks has been detected.

Resolution:
- First check to see if they have wired their ethernet cable into the drives modbus ports.  This normally cause the main display to go blank and control block goes offline.
- Check the internal wiring between the control module line board and the AFE and or BUO's
- Check the LED801 on the control board of the AFE brick) red means communication interruption.
- Change the module link board.