Issue
Unable to upgrade ION meter using ION over Modbus when an ION9000 or PM8000 or ION7400 meter is the Modbus gateway device
Product
ION9000
PM8000
ION7400
Environment
ION9000, PM8000, ION7400 is configured as Modbus gateway with ION meter downstream using ION over Modbus
Resolution
Workaround options at this time
A) Connect directly to the meter, ideally via Ethernet port
B) Use a different gateway device such as PAS, Com'X or EGX. Do not recommend upgrading meter firmware via serial connection when using ION over Modbus.
게시 대상: 슈나이더 일렉트릭 Korea