오늘 무엇을 도와드릴까요?

How to use MSP0200 to create a movement profile?

  1. Issue

Customer needs technical support on the configuration of BMXMSP0200 to control drive.

  1. Product Line
X80 IO module, BMXMSP0200, M340
  1. Environment
Unity Pro, Control Expert, M340
  1. Resolution
Please follow the steps to create a demo application with BMXMSP0200.
1> Create a new application in Unity Pro or Control Expert.
2> Configurate the M340 and BMXMSP0200 in the hardware.
3> Set the parameter of BMXMSP0200.
4> Create the EFB instance as below snapshot indicates.

5> And then build change and transfer the application to the CPU.
6> After all, you can debug this demo application.