오늘 무엇을 도와드릴까요?

Why doesn’t it work when clicking some objects to execute the script in EOTE

  1. Issue
In EOTE runtime, why doesn’t it work when clicking some objects to execute the script.
For example, below script will not work when clicking AlarmSummary1.
  1. Environment
EcoStruxure Operator Terminal Expert 3.1 SP1A.
  1. Resolution
In EOTE, click event doesn’t support all graphic objects.
For information about supported objects, refer to the following.


  1. FAQ Applicable Conditions
FAQ applies to EcoStruxure Operator Terminal Expert 3.1 SP1A.