오늘 무엇을 도와드릴까요?

Can the Altivar ATV16 drive be commanded to do Freewheel stop?

Issue: Can the Altivar ATV16 drive be commanded to do Freewheel stop?

Product Line: ATV16

Environment: All

Cause: N/A

Resolution: Yes. By using PC software assign a logic input for Freewheel stop.