오늘 무엇을 도와드릴까요?

What is the maximum surge current (VA rating) of the relay output modules BMXDRA0805 and BMXDRA0815?

The maximum surge VA rating for the BMXDRA0805 is 1250 VA.
The maximum surge VA rating for the BMXDRA0815 is 2000 VA.

This information was not available in the Modicon x80 Discrete Input/Output Modules User Manuals,
part number 35012474, dated 10/2019 or earlier.