오늘 무엇을 도와드릴까요?

Is there a way to detect when the value of a variable has changed ?

Issue:
Detecting the a change in value of a variable


Product Line:
Unity Pro, EcoStruxure Control Expert


Resolution:
Yes, Attached is a DFB that allow the detection of when a variable of type INT or REAL value has changed

슈나이더 일렉트릭 Korea

첨부 파일
variable_value change detection_dfb.xdb [2.79 KB]