오늘 무엇을 도와드릴까요?

What is the replacement Roof Fan for a ATV660C16T4N2 drive?

Issue:

Where do I find the part number to replace the Roof Fan in an ATV660C16T4N2 drive?


Product Line:

ATV660


Environment:

ATV660C16T4N2


Cause:

Fan stopped working


Resolution:

The roof fan is part # 11681152055 and is system recognized in Q2C and stocked in Seneca.