오늘 무엇을 도와드릴까요?

How do you assign output contactor command to R2 relay on an ATV630 drive?

Issue:
Wants to set R2 for output contactor command

Product Line:
ATV630

Environment:
All

Cause:
Can not assign R2 to output contactor command

Resolution:
To assign R2 to output contactor cmd, first make sure R2 assignment is Not assigned. Then go to Complete Settings / Generic Functions / Output contactor CMD. Then set Output contactor assign to R2.    Then go to Complete settings / Error Warning Handling / Output phase loss, and set Output phase loss assign to "No Error Triggered"