오늘 무엇을 도와드릴까요?

My Site Energy Consumption is not equal to the sum of usages or zones

If the submeters are not metering 100% of the load, the total energy will be lower than the sum of submeters.
If there are sub-sub meters, make sure you do not double count the load:
Example:
  • Main Meter
    • Meter 1
      • Submeter 1.1
      • Submeter 1.2
    • Meter 2
      • Submeter 2.1
      • Submeter 2.2
If you define usage for Meter 1, Submeter 1.1 and Submeter 1.2, you will double count Meter 1 value.
In that case, you should not define usage for Meter 1.

Usages