오늘 무엇을 도와드릴까요?

Upgrading Control Expert 15.0 SP1 to version 15.1

Before Control Expert 15.0 SP1 can be updated to version 15.1, the following steps must be performed.
  • Export current projects from the project file format (*.STU) into an archive application file format (*.STA).
  • Save the custom libraries.
  • Save any private ASI catalogs.
  • Uninstall Control Expert 15.0 SP1.
  • Reboot the PC.
  • Install Control Expert 15.1.
  • Reboot the PC.
Note: If the reboot steps are not performed, the installation will have problems.