SchneiderElectric_KBA_Basic_Meter_PM55xx Russian Language files issue
SchneiderElectric_KBA_Basic_Meter_PM55xx Russian Language files issue
Problem statement :
Pm5560 Meter set to Russian language, the Panel data is not visible and some of data labels are not visible in different screen navigations.
Causes identified :
- This data label missing or data is missing in PM55xx when the Meter is set to the Russian language.
- This is due to an issue with the Russian language file used within PM55xx.
- This issue is noticed with Pm55xx with firmware versions below 4.1.3
Solution :
- This issue is fixed in Firmware version 4.1.3 onwards. So the meter needs to be upgraded to this Firmware version.
게시 대상: 슈나이더 일렉트릭 Korea