오늘 무엇을 도와드릴까요?

How do I set the target's brightness level to 50% on startup via scripting in Vijeo Designer?

Issue:
Adjusting a target's brightness level to 50% on startup via scripting in Vijeo Designer?


Product Line:
Vijeo Designer


Resolution:
The script example below sets the target's brightness level to 50% on startup
_Brightness.write(_Brightness.getMax() / 2);