Cannot activate Control Expert without Internet access.
If the PC does not have Internet access, Control Expert can also be activated using either phone or the web portal. (see following instructions)
NOTE: For activation by phone you need the Entitlement Certificate of the software product to be activated ready to hand.
Activation of Licenses by phone
NOTE: You may have to restart your software product in order to detect this change in license configuration.
Activation of license by Web Portal
Complete Transaction Procedure
NOTE: You may have to restart your software product in order to detect this change in license configuration.
NOTE: For activation by phone you need the Entitlement Certificate of the software product to be activated ready to hand.
Activation of Licenses by phone
| Step | Action |
|---|---|
| 1 | Start the Schneider Electric License Manager. |
| 2 | In the Local tab click the Activate button. Result: The Activation Method dialog opens. |
| 3 | Select By phone as activation method. Result: In the text box a short procedure description of this method is displayed. You can print this short procedure description using the Print button. |
| 4 | Click the Next button. Result: The Product Selection dialog opens. |
| 5 | Select the software product to be activated from the list. Verify that you select the correct Version and Duration for the product. |
| 6 | Click the Next button. Result: The Call Software Registration Center dialog opens. |
| 7 | Make sure that the Entitlement Certificate is ready at hand. |
| 8 | Call one of the Software Registration Centers listed in the text box of the Call Software Registration Center dialog. |
| 9 | Click the Next button. Result: The Complete Activation dialog opens. |
| 10 | Follow the instructions of the Software Registration Center operator. The operator needs the following information:
|
| 11 | The operator returns the Short Code Response to you. |
| 12 | Enter the Short Code Response in the Complete Activation dialog. |
| 13 | Click the Next button. Result: The Finished Activation dialog opens. Information on the software product activated during this session is displayed. |
| 14 |
|
NOTE: You may have to restart your software product in order to detect this change in license configuration.
Activation of license by Web Portal
| Step | Action |
|---|---|
| 1 | Start the Schneider Electric License Manager. |
| 2 | In the Local tab click the Activate button. Result: The Activation Method dialog opens. |
| 3 | Select By web portal as activation method. Result: In the text box a short procedure description of this method is displayed. You can print this short procedure description using the Print button. |
| 4 | Click the Next button. Result: The Activation ID dialog opens. |
| 5 | Enter the Activation ID which can be found in the Entitlement Certificate of the software product to be activated. If you want to activate multiple software products, you have to enter the different Activation IDs in separate lines. Result: The Next button is activated. |
| 6 | Click the Next button. |
| 7 | Select the directory where the XML request file should be saved. NOTE: If you want to connect to the Software Licensing Web Portal on another PC it is recommended to save the XML request file on a portable medium (e.g. USB stick). |
| 8 | Click the Next button. Result: The How to Continue dialog opens. |
| 9 | In the text box a short procedure description of how to continue is displayed. This description contains a URL address you need to connect to the Software Licensing Web Portal. NOTE: If you want to connect to the Software Licensing Web Portal on another PC it is recommended to also save this URL address on a portable medium (e.g. USB stick). |
| 10 | Click the Next button. Result: The Complete Transaction dialog opens. To be able to continue you first have to retrieve the XML response file from the Software Licensing Web Portal (see next table). |
Complete Transaction Procedure
| Step | Action |
|---|---|
| 1 | Return to the PC with the software product to be activated. If you closed the Schneider Electric License Manager you have to re-start it and click the Complete button in the Local tab. Result: The Complete Transaction dialog opens (or is still opened). |
| 2 | Locate the received XML file (e.g. on a USB stick or a hard drive) and click the Open button. |
| 3 | Click the Next button. Result: The Complete Transaction dialog opens. In the text box information about the internal processing of license activation is displayed. |
| 4 | After the license is successfully created, click the Finish button. Result: The Local tab of the Schneider Electric License Manager is displayed showing each activated license in a new line. |
NOTE: You may have to restart your software product in order to detect this change in license configuration.
게시 대상: 슈나이더 일렉트릭 Korea