브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
		
오늘 무엇을 도와드릴까요?
How can I upgrade the firmware of a BMEAHI0810 module with a PC located on the Control Network of the BMENOC0321 ?

The gateway address of the BMEAHI0810 module must correspond to the IP address of the fieldbus network managed by the BMENOC0321.

For example, in the Ethernet Network Manager screen shown below, the gateway of the AHI module is set to the IP address of the router:


BMEAHI0812, Gateway,BMENOC0321

In the BMEAHI0812 DTM instance, you need to enable the option "Firmware upgrade"  as follow :

EnableFirmwareUpgrade

And always perform a transfer to FDR server after each modification of the BMEAHI0812 DTM instance.
Next, open Unity Loader and connect to the IP address of your BMEAHI0812 module to perform the upgrade :


BMEAHI, upgrade,Unity Loader