오늘 무엇을 도와드릴까요?

Does Vijeo Designer support SMTPs (Simple Mail Transfer Protocol Secure)?

The Latest versions of Vijeo Designer include new features to be compliant with the Cybersecurity.
The goal of this article is to inform about SMTPs (Simple Mail Transfer Protocol Secure) support from the version VJD 6.2 SP12.

This article is applicable to the following products:
Harmony P6, HMIGTU, HMIGTO, HMISTU, iPC, XBTGT.

This topic is related to Vijeo Designer

From Vijeo-Designer V6.2 SP12, SMTPs (Simple Mail Transfer Protocol Secure) has also been implemented to replace SMTP for email operations. SMTPs encrypts email content to protect the data against sniffing. SMTPs encrypts data transmitted over network to protect the data against sniffing.
SMTPs operation follows the same procedure as SMTP, there are no extra and special configuration required.