Can the OPCUA client function block in Control Expert access the OPCUA server module BMENUA0100 via the backplane port?
Issue:
OPCUA client function block in Control Expert accessing the OPCUA server module BMENUA0100 via the backplane port
Product Line:
EcoStruxure Control Expert
Resolution:
No. The OPCUA client function block can access the UA server only by the external port of the BMENUA0100 module or the embedded Ethernet port of the CPU
OPCUA client function block in Control Expert accessing the OPCUA server module BMENUA0100 via the backplane port
Product Line:
EcoStruxure Control Expert
Resolution:
No. The OPCUA client function block can access the UA server only by the external port of the BMENUA0100 module or the embedded Ethernet port of the CPU
게시 대상: 슈나이더 일렉트릭 Korea