오늘 무엇을 도와드릴까요?

Does the PMEPXM0100 support multi-master Profibus architectures?

Yes the PMEPXM0100 supports multi-master Profibus architectures..
For example, it's possible to connect many PMEPXM0100 on the same Profibus network.
For information, the Premium Profibus master TSXPBY100 supports also the multi-master Profibus network.