Structure diagram for the PIDFF mixed mode is missing from the help.
The complete structure diagram for the PIDFF is shown below (Note: Reference the Control Expert online help for more information pertaining to the detailed equations relative to the structure diagram):