브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
		
오늘 무엇을 도와드릴까요?
DCE shows duplicate cameras for a single NetBotz 750/755 attached camera
Issue:
DCE shows duplicate cameras for a single NetBotz 750/755

Product Line:
Data Center Expert
NetBotz

Environment:
DCE (any version)
NBRK0750
NBWL0755
NBPD0165

Cause:
If you Remove a NetBotz 750 or 755 from DCE and that appliance had a connected camera, the camera will not get deleted from DCE surveillance.
The camera will appear as disconnected and show a test pattern. Re-adding the appliance even with the same camera re-adds the camera with a separate internal ID so DCE won't associate it with the newly added NetBotz.

Resolution:
After removing a NetBotz 750 or 755 with a connected camera from DCE, it is recommended that you delete the camera from the surveillance view in DCE.
If you do not, after you re-add the NetBotz even with the same camera, that camera will show as a duplicate and only one camera will actually capure clips going forward.

You should still be able to delete the camera after re-adding the appliance as you will see one communicating and one not communicating. Delete the non-communicating camera.