Does Schneider Electric have Bi-directional Power meter?
Yes, the following meters:
EasyLogic™ PM2000 Power Meters,
PowerLogic™ PM5000 Power Meters
PowerLogic™ PM8000 Power Quality Meters
All have bi-directional energy measurement feature i.e it will give energy import/delivered and energy export/received. Positive real power P(+) flows from the power source to the load. Negative real power P(-) flows from the load to the power source.
게시 대상: Schneider Electric have Bi-directional Power meter? | 슈나이더 일렉트릭 Korea