1. Issue :
Which X80 backplanes could be used to diagnose and control Redundant Power Supply ?
2. Product Line :
M580
3. Environment
All supported Windows OS
4. Resolution
Redundant power supply racks ,BMEXBP0602(H) and BMEXBP1002(H) ,could be allowed to diagnose and control Redundant Power Supply via PWS_DIAG and PWS_CMD.
게시 대상: 슈나이더 일렉트릭 Korea