1. Issue :
Why event ID in TS event buffer could have number 16 ?
2. Product Line :
BMXERT1604T ,BMXCRA31210, BMECRA31210
3. Environment
All supported Windows OS
4. Resolution
Event with ID 16 (SOE_UNCERTAIN ) is used to indicate that some events may be lost in the next sequence of events and user needs to check the why the TS buffer of BMXERT1604T (or BMxCRA31210) reaches full state.
게시 대상: 슈나이더 일렉트릭 Korea