오늘 무엇을 도와드릴까요?

Control Expert v15.3 crash when displaying on ultra wide screen resolution 5120 * 1440

1- Issue:
Control Expert v15.3 crash when displaying on Ultra Wide screen resolution 5120 x 1440.

2- Product Line
Control Expert v15.3

3- Environment:
Windows 10

4- Resolution:
The maximum supported resolution for Control Expert v15.3 is 2560 x 1440 with Scale and Layout at 125%.
The resolution 5120 x 1440 will be supported in Control Expert v16.0