오늘 무엇을 도와드릴까요?

Incorrect Battery Capacity Displaying for SRVL48RMBP2U

Issue:

This document explains how to resolve the incorrect battery capacity being reported by the SRVL48RMBP2U.

Product Line:

Easy-UPS Li-ion Online

Cause:

The incorrect battery capacity displays on the Easy-UPS Li-ion when connected to SRVL48RMBP2U.

Resolution:
Upgrade the UPS firmware version to V02.2 or later. Firmware file and upgrade procedure are attached to this FAQ.

슈나이더 일렉트릭 Korea

첨부 파일
Easy UPS Li-ion Firmware 2.2.zip [4.76 MB]