오늘 무엇을 도와드릴까요?

How to transfer a %M using a WRITE_VAR

The following logic can be used to transfer a %M variable over Modbus TCP/IP using a WRITE_VAR block.
The BOOL_TO block is used to convert the %M type BOOL to the EMIS variable of type INT.


ghjk