오늘 무엇을 도와드릴까요?

Getting Monitor Circuit error A, B, C or D on a Altivar Process drive

Issue:

Getting a Monitor Circuit error A, B, C or D

Product Line:

ATV930

Environment:

Digital inputs

Cause:

n/a

Resolution:

Suggested to check the digital inputs to see if one of them is assigned to Monitor Circuit A,

B, C or D (Example: if a surge arrestor is assigned to the digital input and is damaged) can cause this.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.